Axis Overview

Selecting an Axis in the navigation tree display the Axis Overview screen.

You can view or edit the following information from the Overview window.

Button or Dialog Box

Description

Parameter

Parameter

Index Displays which axis (1 or 2) is selected.    

Name

Names each axis in use with a unique identifier.

 

AXIS#.NAME

Axis State

The axis is active when it is enabled and also supplies voltage to the motor.

DRV.ACTIVE

AXIS#.ACTIVE

Enable

Click Enable to turn on the power stage in the drive and apply voltage to the motor. This command may fail for many reasons (see AXIS#.EN for further details).

DRV.ENDEFAULT

AXIS#.EN

Disable

Click Disable to turn off the power stage and remove the voltage applied to the motor.

DRV.ENDEFAULT

AXIS#.DIS